RuralTap

Taps are used to provide service connections on gas pipes and mains. Rural Tap represents supply from transmission pipe.

RuralTap inherits characteristics from the abstract class GasDevice.

Subtypes: None

Associations: Meter, Regulator, Odorizer

Model Names: None

Attributes:

Field Name

Field Type

Description

InstallationDate

date

Date of installation.

Manufacturer

text

Code indicating manufacturer.

Model

text

RuralTap model number specified by manufacturer.

OdorizerIndicator

text

Code indicating presence of odorizer; domain values include Yes and No.

PipeLineOperator

text

Code indicating pipeline operator; domain values include American Natural Resources, Entex, etc.

PipeLineStation

text

Pipeline station associated with StationStructure.

ShutOffValveDiameter

text

Diameter of shutoff valve associated with Rural Tap; domain values include ¼”, 5/8”, 12”, 26”, etc.

ShutOffValveType

text

Code indicating type of valve; domain values include Ball Valve, Check, Gate Valve, Wafer, etc.

TapDiameter

text

Diameter of tap.

TapType

text

Type of tap.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.