StationStructure

StationStructures protect and provide access to above ground gas devices and facilities.

Vault inherits attributes from the GasStructure abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

PipeLineOperator

text

Code indicating pipeline operator; examples include American Natural Resources, Midcon, etc.

PipeLineStation

text

Pipeline station associated with StationStructure.

SymbolRotation

double

Angle that dictates how the feature appears on map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.