SqueezeOff

A SqueezeOff represents a section of pinched pipe.

Gas tracing requires the SQUEEZEOFF class model name and is used to determine whether pinching the pipes at selected locations will isolate an area.  

Subtypes: None

Associations: Meter

Model Names: SQUEEZEOFF

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

NormalPosition

long integer

Normal position of GasValve; domain values include Open and Closed.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

Subtype

Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.