Interpretation of FeederSourceInfo Values

The FeederSourceInfo field indicates whether a given feeder has features that participate in either loops or multifeed situations. The following table may be used to interpret FeederSourceInfo values.

Value

Description

0

Nothing special

1

Has multifeed features

2

Has loop features

3

Has both loop and multifeed features

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.