Initial or Reelback Tension

The initial or reelback tension is the tension required to pull the cable from the reel while the reel is moving. This tension varies with a number of factors, the most influential being the phase conductor size and weight. However, the amount of cable on the reel, the manner in which the cable is unwound, and the ability of the reel to spin freely all play an important role in determining this value. Due to the virtually unlimited values these factors may assume, it is extremely difficult to accurately predict the initial or reelback tension.

The following table provides a rough estimate of the initial or reelback tension for a specified phase conductor.

Phase Conductor

Reelback Tension (lb)

Primary Aluminum

#2, 7 strd AL CN 15 KV XLP

#1/0, 19 strd AL CN 15 KV XLP

#4/0, 19 strd AL CN 15 KV XLP

3-750, KCM, 61 strd AL 15 KV XLP w/ #4/0 bare CU neut

3-1000 KCM, 61 strd AL 15 KV XLP w/ #4/0 bare CU neut

50

50

60

0*

0*

Primary Copper

all PILC cable
3-500 KCM, 37 strd CU 15 KV XLP w/ #4/0 bare CU neut
3-750, KCM, 61 strd AL 15 KV XLP w/ #4/0 bare CU neut

0*

0*

0*

Secondary Aluminum

#1/0, 19 strd AL 600 V XLP & triplex
#4/0, 19 strd AL 600 V XLP & triplex
350 KCM, 37 strd AL 600 V XLP & triplex
500 KCM, 37 strd AL 600 V XLP & triplex
750 KCM, 37 strd AL 600 V XLP & triplex
750 KCM quadruplex

40

40

45

45

50

50

Secondary Copper

#2, 7 strd CU 600 V XLP
#1/0, 19 strd CU 600 V XLP
#2/0, 19 strd CU 600 V XLP
#4/0, 19 strd CU 600 V XLP
350 KCM, 37 strd CU 600 V XLP
500 KCM, 37 strd CU 600 V XLP
750 KCM, 61 strd CU 600 V XLP

45

45

50

50

55

55

60

* A motorized reel must be used because of the cable weight.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.