Recloser Hydraulic Control

Hydraulic control is an integral part of single-phase reclosers. A trip coil in series with the line is used to sense overcurrent and trip open the recloser contacts. The contacts close after a preset interval.

Associations: None

Subtypes: None

Model Names:

Attributes:

Field Name

Field Type

Description

CoilSize

short integer

Code indicating size of trip coil in amps; domain values include 25 amps, 50 amps, etc.

RecloseInterval

long integer

Amount of time before reclosing between operations.

ResetTime

long integer

Amount of time Recloser resets to beginning of operation sequence.

TCC1Operations

long integer

Number of trips per curve for slow trip.

TCC2Operations

long integer

Number of trips per curve for fast trip.

TCC1Selection

long integer

Specific curve selected for slow trip.

TCC2Selection

long integer

Specific curve selected for fast trip.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.