Abandoned Electric Line Segment

This feature class is created to maintain information about abandoned conductors. Attributes of this feature class are user-defined and depend on which field values need to be maintained after a feature is abandoned.

The model names are assigned depending upon how you wish to abandon features to the AbandonedElectricLineSegment feature class. Use MMABANDONED to identify AbandonedElectricLineSegment as the feature class in which abandoned features are stored. Use MMREMOVED to identify AbandonedElectricLineSegment as the feature class in which abandoned and removed features are stored. Use MMABANDONRELATE to identify AbandonedElectricLineSegment as the feature class in which abandoned features with related objects are stored.

Attribute values to be transferred from the abandoned feature class to the AbandonedElectricLineSegment class are designated using the field model name with a prefix of AT_ (e.g., AT_MATERIAL).

Associations: AbandonedElectricLineSegment

Subtypes: Primary Overhead, Primary Underground, Secondary Overhead, Secondary Underground, and Streetlight Conductor. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: MMABANDONED, MMREMOVED, MMABANDONRELATE

Attributes:

This class may contain any fields present on the OverheadElectricLineSegment class (Primary or Secondary) or the UndergroundElectricLineSegment class (Primary or Secondary).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.