Open Point

OpenPoint contains information about a variety of insulated and shielded devices that connect high-voltage cables to apparatus including transformers. Separable, load-break insulated connectors are used with primary bushings of submersible distribution transformers for safety. This is known as a dead-front configuration.

The OpenPoint class inherits attributes from the ElectricDevice abstract class. All model names assigned to the ElectricDevice class should be assigned to the OpenPoint class as well.

Associations: None

Subtypes: Load Break Elbow, Non-Load Break Elbow, Open Point, Solid Connection, Splice, Terminator. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: SWITCH

Attributes:

Field Name

Field Type

Description

Configuration

text

Configuration of connection such as Wye, Delta, etc.

Manufacturer

text

Manufacturer of OpenPoint.

Model

text

Model of OpenPoint.

NormalPosition[A,B,C]

long integer

Code indicating normal position of OpenPoint, per phase; domain values include Closed, Open, and Not Applicable. This attribute results in three fields (NormalPosition_A, NormalPosition_B, NormalPosition_C). Assign the corresponding model name to each field: NORMALPOSITION_A, NORMALPOSITION_B, NORMALPOSITION_C.

PresentPosition[A,B,C]

long integer

Code indicating present position of OpenPoint, per phase; domain values include Closed, Open, and Not Applicable.

SpliceSize

text

Code indicating size of Splice; domain values include 1/0 AWG, 1000 MCM, etc.

TransformerObjectID

long integer

ObjectID of associated transformer unit.

VoltageRegulatorObjectID

long integer

ObjectID of associated voltage regulator.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.