ExposedPipeInspection

ExposedPipeInspection refers to inspection of gas pipes, specifically those that are exposed.

Subtypes: None

Associations: Coupon, PipeExposure

Model Names: None

Attributes:

Field Name

Field Type

Description

CoatingCondition

text

Description of coating condition.

Comments

text

User or designer comments.

DistributionMainObjectID

long integer

ObjectID of associated DistributionMain.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InspectionDate

text

Date of last inspection.

InspectionNumber

text

Description of coating condition.

Inspector

text

Name of inspector during last inspection.

InstallationDate

date

Date of installation.

PipeDepth

text

Depth of pipe.

PittingDepth

text

Depth of pitting.

PipeExposureObjectID

long integer

ObjectID of pipe exposure.

RepairOrderRequiredIndicator

text

Code indicating whether repair order is required; domain values areYes and No.

SoilType

text

Type of soil in which pipe is buried.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.