Facility Structure

FacilityStructure is an abstract class containing common attributes of the EquipmentEnclosure abstract class and the SupportStructure feature class (Hframes, poles, towers). EquipmentEnclosure includes these feature classes (and subtypes): SurfaceStructure (pads, pedestals, connection boxes), ElectricStation (main, net, substations), and SwitchingFacility (junction cabinets, switchboards).

FacilityStructure inherits attributes from the Structure abstract class.

Attributes:

Field Name

Field Type

Description

Alternate[X,Y,Z]

double

Stores the X, Y, and Z values from a GPS device.

AlternateSource

text

This field contains a value from the Feature Source domain that indicates an alternate source for the structure.

FacilityID

text

Meaningful company-assigned unique identifier. Many ArcFM tools use the FACILITYID model name on this field.

Owner

text

Code indicating owner of structure. Domain values include: Customer Owned, Local Bell, Power Company, Other Utility.

Subtype

long integer

Code indicating the type of structure.

SymbolRotation

double

Angle of rotation indicating how a feature appears on the map. Uses the SYMBOLROTATION model name. The ArcFM Manual Angle Setter edit task and ArcFM Auto Angle Setter autoupdater both use this field to rotate point features

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.