International Data Model

In addition to the attributes listed in Electric Line Segment, the following attributes are used by the international electric data model.

Field Name

Description

CapacityToGround

The capacitive reactance to neutral or earth of any line segment (ohms per map unit length).

ConductorMaterial

Material of which the conductor is made.

ConductorSize

Size of the conductor.

ConnectionOKIndicator

Indicates whether a line segment is capable of and ready for connection to a load or other line segment.

InsulationType

Insulation type of conductor.

InsulationVoltage

Withstand voltage of the conductor's insulation (Volts).

MaxContinousCurrent

Continuous current rating of conductor (Amperes).

NumberConductorPerPhase

Number of conductors per phase.

OuterDiameter

Outer diameter of conductor.

OutOfOrderIndicator

Indicates whether a line segment is de-energized (for example, out of service for maintenance).

RatedCurrent

Continuous current rating of conductor, including any de-rating required for special conditions (Amperes).

Reactance

Positive sequence reactance of conductor (ohms per map unit length).

Resistance

Positive sequence resistance of conductor (ohms per map unit length).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.