MainJobSeparator

MainJobSeparator represents the beginning and end points for jobs performed on pipe.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate. To support Gas Tracing and Feeder Manager, the model name GASTRACEWEIGHT is required for every feature class belonging to ArcFM gas networks.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date pipe set in service.

InstallationDate

date

Date of installation.

SubType

long integer

Code indicating type of GasPipe; examples include Distribution Main and Service.

SymbolRotation

double

Angle that dictates how the feature appears on the map.

WorkOrderID

text

Utility-defined identifier of work order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.