How to Assign Permissions to System Tables

ArcFM geodatabases contain the following essential tables, which are created by running the Create/Update ArcFM Solution System Tables function:

  • MM_CLASS_MODELNAMES

  • MM_DOCUMENTS

  • MM_EDITED_FEATURES

  • MM_FIELD_MODELNAMES

  • MM_MOBILE_IMPORT_ORDER

  • MM_PACKAGES (also MM_HIDDEN_PACKAGES if available)

  • MM_PAGE_TEMPLATES

  • MM_PERSIST_INFOMM_QAQC

  • MM_SNAPPING

  • MM_STORED_DISPLAYS

  • MM_SYSTEM_DOCUMENTS

  • MM_SYSTEM_PACKAGES

  • MM_SYSTEM_PAGE_TEMPLATES

  • MM_SYSTEM_PERSIST_INFO

  • MM_SYSTEM_STORED_DISPLAYS

These tables store important configuration information for the use and management of Stored Displays, model names, snapping, etc.

Permissions to these tables should be assigned to two roles: 

  • The mm_admin role should be assigned Write permission to all these tables. 

  • The mm_user role's permissions should be as follows:

    • Read:

      • MM_CLASS_MODELNAMES

      • MM_FIELD_MODELNAMES

      • MM_MOBILE_IMPORT_ORDER

      • MM_QAQC

      • MM_SNAPPING

      • MM_SYSTEM_DOCUMENTS

      • MM_SYSTEM_PACKAGES

      • MM_SYSTEM_PAGE_TEMPLATES

      • MM_SYSTEM_PERSIST_INFO

      • MM_SYSTEM_STORED_DISPLAYS

    • Write:

      • MM_DOCUMENTS

      • MM_EDITED_FEATURES

      • MM_PACKAGES (also MM_HIDDEN_PACKAGES if available)

      • MM_PAGE_TEMPLATES

      • MM_PERSIST_INFO

      • MM_STORED_DISPLAYS

As always, assigning these table permissions should be performed in ArcCatalog and the database should be backed up before any changes are made.

TIP: To check or change permission on MM_ tables, In ArcCatalog connect to the database as the SDE user. Then right click on the table > Manage > Privileges.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.