Service Point

ServicePoint is the point at which the distribution feeder terminates and energy is supplied to a customer. A service point can have one or many meters.

Designer Secondary Circuit Analysis requires the SERVICEPOINT model name on this class.

Responder uses the FDRMGRLOADPOINT model name on this class. Future Feeder Manager functionality may take advantage of this model name as well.

Associations: InductionMotor, SynchronousMotor

Subtypes: None

Model Names: SERVICEPOINT, FDRMGRLOADPOINT

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Status

text

Code indicating status of ServicePoint; domain values include Active and Inactive.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.