Lifecycle History

LifecycleHistory is an abstract object provided so that administrators can relate information about the history of particular devices or equipment. This information is related to devices that have a spatial reference but is itself nonspatial. Define specific LifecycleHistory objects on an as-needed basis. As a new LifecycleHistory object is defined, you should also define any necessary relationships.

Subtypes: None

Associations: To be defined by user

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FacilityID

text

Meaningful company-assigned unique identifier.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

WorkFunction

text

Code indicating life cycle phase; domain values include Install, Remove, Replace, Transfer, Retire, and Abandon.

WorkOrderID

text

Utility identifier of work order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.