Transformer Unit

Transformers transfer electrical energy from one circuit to another circuit usually with changed values of voltage and current in the process.

Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.

The ArcFM Synch Transformer Unit Phase Designation autoupdater, Phase on Bank Unit QA Validation rule, and RatedKVA on Transformer QA Validation rule all use the TRANSFORMERUNIT model name. The ArcFM Phase Swap tool and Display Name objects also require the TRANSFORMERUNIT model name.

Associations: RegulatorControl (only valid for VoltageRegulator), Transformer

Subtypes: Distribution Transformer Unit, Power Transformer Unit, Voltage Regulator Unit. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: DESIGNUNIT, TRANSFORMERUNIT

Attributes:

Field Name

Field Type

Description

AnimalGuardType

text

Type of animal guard used on TransformerUnit.

ArrestorType

text

Code indicating arrestor type; domain values include Air Gap, Metal Oxide, etc.

Available

text

Code indicating whether TransformerUnit has capacity available; domain values are Yes or No.

CoolingType

text

Code indicating cooling method used in TransformerUnit; domain values include Radiator Forced Air and Other.

FluidType

text

Type of fluid used.

FullLoadLosses

double

Full-load losses of TransformerUnit in watts.

HighSideRatedVoltage

long integer

Code indicating system voltage for which high side of TransformerUnit is rated; domain values include 2400 Volts Delta, 4160/2400 Volts, etc.

HighSideBIL

long integer

Code indicating BIL rating of high side of TransformerUnit; values include 125 BIL, etc.

Impedance

double

Impedance of TransformerUnit, expressed as percentage.

LowSideRatedVoltage

long integer

Code indicating system voltage of low side of TransformerUnit; domain values include 120 volts, 120/208 volts, etc.

LowSideBIL

long integer

BIL rating of low side of TransformerUnit.

LowSideTaps

text

Number of taps available on low side of TransformerUnit to change transformer ratio.

Manufacturer

text

Manufacturer of TransformerUnit; domain values include ABB/Westinghouse, General Electric.

MaxSteps

text

Maximum number of steps available on TransformerUnit.

NoLoadLosses

double

No-load losses of TransformerUnit in watts.

PCBLevel

double

PCB level, if any, in coolant of TransformerUnit; domain values include Arachlor, Diachlor, etc.

ProtectionType

text

Code indicating type of protection; domain values include Bayonet Fused, Conventional, etc.

RatedKVA

long integer

kVA of TransformerUnit at nominal voltage; domain values include 10 kVA, 112 kVA, 333 kVA, etc. The ArcFM Phase Swap tool, Display Name objects, and the RatedKVA on Transformer QA Validation rule both require the RATEDKVA model name on this field.

SCADAIndicator

text

This field contains a value from the Yes/No Indicator domain that indicates whether a SCADA device exists on the transformer.

TapsType

text

Code indicating type of taps; domain values include 2Above/2Below, 4Above, etc.

TransformerObjectID

long integer

ObjectID of associated transformer.

XRRatio

double

Inductance/resistance ratio.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.