LeakSurveyArea

LeakSurveyArea is a general use polygon that describes areas of leak survey by due date.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

DueDate

date

Date survey is due to be performed.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

LastSurveyDate

date

Date of last survey.

LeakSurveyDueDate

date

Due date of LeakSurvey.

LeakSurveyFrequency

text

Code indicating frequency of leak survey; domain values include 3 Months, 12 Months, 36 Months, etc.

SurveyAreaType

text

Type of survey area.

TargetMonth

text

Target month that survey is to be performed.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.