RegulatorStation

A regulator station defines the location of one or more pressure regulators.

The INSETFRAMEOBJECT model name is used in configuring ArcFM Inset Frames. The REGULATOR model name is used for gas tracing functions.

RegulatorStation inherits properties from GasStation and GasDevice abstract classes.

Subtypes: None

Associations: None

Model Names: REGULATOR

Attributes:

Field Name

Field Type

Description

EmerIsolationSysObjectID

long integer

ObjectID of Emergency IsolationSystem of RegulatorStation.

GasPressureSystemObjectID

long integer

ObjectID of GasPressureSystem of RegulatorStation. If GASPRESSURESYSTEMSTATUS exists, this field value will be used to specify if the device is a gas pressure system boundary.

GasSystemObjectID

long integer

ObjectID of GasSystem of RegulatorStation.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.