GasPipeCasing

Gas pipe casing is a conduit through which a gas pipe may be placed. Casings provide gas pipes with protection from undue stress or abrasion.

Subtypes: None

Associations: GasPipe

Model Names: None

Attributes:

Field Name

Field Type

Description

CasingDiameter

long integer

Code indicating size of GasPipeCasing; domain values include 2”, 8”, 30”, etc.

CoatingType

text

Code indicating type of GasPipeCasing coating; domain values include Bare, Coal Tar Enamel, Paint, etc.

Comments

text

User or designer comments.

EndConnection

text

Code indicating type of End Connection; domain values include Boot, Homemade, Link Seals, etc.

FillDate

date

Date GasPipeCasing was filled.

FillType

text

Type of material used for fill; domain values include Dielectric Fluid Filled and Not Filled.

GallonsOfFill

long integer

Quantity of filled used, in gallons.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

date

Date pipe set in service.

InstallationDate

date

Date of installation.

LengthSource

text

Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived.

LocationDescription

text

Verbal description of location of GasPipeCasing.

Material

text

Material of GasPipeCasing.

MeasuredLength

double

Method used to determine length of GasPipe; domain values include FieldMeasurement, Mapping System, and User-Derived.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

ProtectionType

text

Code indicating type of cathodic protection employed; domain values include Anode, None, and Rectified.

Reason

text

Code indicating reason for casing; domain values include Highway, Railroad, and Street.

VentedIndicator

text

Indicates presence of ventilator; domain values are Yes and No.

WorkOrderID

text

Utility-defined identifier of work order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.