Surface Structure

SurfaceStructure contains objects that protect or enclose electric circuits and equipment on the ground. SurfaceStructure inherits attributes from the Structure abstract class.

Subtypes: Connection Box, Enclosure, Mat, Non-Electric Enclosure, Pad, Pedestal. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Associations: None

Model Names: STRUCTURE

Attributes:

Field Name

Field Type

Description

Manufacturer

text

Manufacturer of support structure.

Material

text

Code indicating material of structure; domain values include Aluminum, Fiberglass, Wood, etc.

Model

text

Model type of SurfaceStructure.

Name

text

Name of SurfaceStructure.

StructureSize

text

Size of SurfaceStructure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.