Circuit Source ID

This table stores the ultimate sources defined in the CircuitSource object class as well as the subsources defined in a multi-tiered network. This table is required ONLY for Extended Feeder Manager.

Attributes:

Field Name

Field Type

Description

FeederLevel

long integer

A value indicating the feeder level. A feeder level consists of all connected features with the same voltage level. This voltage level is determined by the exiting voltage from a subsource. All connected downstream features with that same voltage are considered a feeder level.

FeederName

text

This field contains the name assigned to the feeder.

ParentCircuitSourceID

long integer

This field contains a value that identifies the parent circuit source to the electric device. This field is required by Extended Feeder Manager.

RelatedFeatureClassName

text

The feature class name for the related object.

RelatedObjectID

text

A unique ID that identifies the related object.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.