CPBondJunction

In cases where plastic pipe connects two metal pipes, bonding wire is used to maintain the electrical connectivity throughout the cathodic protection system. The CPBondJunction is a location where two to four bonding wires come together.

You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPBondJunction feature class.

CPBondJunction acquires properties from the CathodicProtectionDevice abstract class.

Subtypes: None

Associations: CPBondWire

Model Names: GASNONTRACABLE

Attributes:

Field Name

Field Type

Description

BondJunctionType

text

Code indicating type of bond junction; examples include Above Ground, Above Ground with Foreign Line, and Curb Box Bond.

CPBondWireObjectID

long integer

Object ID for bonding wire used in bond junction.

CriticalIndicator

text

Code indicating whether bond wire is essential to maintain connectivity; domain values are Yes or No.

ResistanceIndicator

text

Code indicating whether CPBondJunction has resistance; domain values are Yes or No.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.