CPTestPoint

CPTestPoint represents the test point or read point locations along a gas pipe used to test the current status of the cathodic protection system.

CPTestPoint acquires properties from the CathodicProtectionDevice abstract class.

Subtypes: None

Associations: None

Model Names: GASNONTRACABLE, TESTPOINT

Attributes:

Field Name

Field Type

Description

CPSystemObjectID

long integer

ObjectID of associated CPSystem.

Name

text

Utility-assigned name of feature.

NextTestDate

date

Date of next test.

TestPointType

text

Code indicating type of CPTestPoint; domain values include Above Ground, Buried, and On Post.

WireCount

text

Number of wires associated with test point; domain values are One Wire, Two Wires, and Unknown.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.