Conduit System

The underground system consists of ducts, direct buried cables, or pipes extending between vaults or manholes. New conductor and telephone cable are often installed underground in congested areas. Conductors and cables can be drawn or pulled from manhole locations for repairs or changes.

Conduits, or underground linear structures, are constructed of materials that are impervious to water and do not degrade or corrode easily. Cable also may be buried directly in trenches, which ArcFM models as a ConduitSystem feature. In this case, ducts are used as placeholders for the position of cables and conductors associated with the trench. Cables are associated with conduits through an attributed relationship class called ConduitSystem_ConduitSystemMember Cross Reference. The user creates this relationship class to relate feature classes with model name ULS to feature classes with model name ULSMember. 

The ConduitSystem feature class contains information about the position and characteristics of ducts as seen from a manhole, vault, or cross section of a trench and duct. Users can create duct characteristic fields to represent their business processes. Common materials are concrete, plastic, and fiberglass. Common duct diameters are three to five inches. Names of characteristics such as material or size are assigned by the user when creating the Duct Definition object class. This table contains only field names that describe the duct. The values of these fields, such as steel or five inches, are stored for each duct in a COM object, which is stored in the Configuration attribute field of the ConduitSystem feature class.

Subtypes: Duct Bank, Trench. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Associations: UndergroundStructure

Model Names: ULS

Attributes:

Field Name

Field Type

Description

BuriedDepth

text

Depth from top of conduit to ground line.

Comments

text

User or designer comments.

Configuration (see DuctDefinition)

BLOB

Stores information about duct or position layout within the conduit in a COM object; stores the values of attribute fields created in Duct Definition object class. Conduit Manager uses the DUCTBANKCONFIGURATION model name on this field to designate it as the BLOB field in which the layout information is stored.

ConstructionStatus

ong integer

This field contains a value from the Construction Status domain that indicates the current status of construction on the structure (e.g., proposed, existing, retired).

DuctBankHeight

long integer

Stores the height of the duct bank. Underground Facility Manager uses the DUCTBANKHEIGHT model name on this field.

DuctBankWidth

long integer

Stores the width of the duct bank. Underground Facility Manager uses the DUCTBANKWIDTH model name on this field.

EncasementType*

text

Code indicating encasement type; domain values include Backfill, Concrete, and Unknown.

FacilityID

text

Meaningful utility-assigned unique identifier.

Height*

double

Height of the conduit system.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

LabelText

text

Stores a string to label conduit on map.

LengthSource

text

Source of length measurement; domain values are Mapping System and Field Measurement.

Manufacturer*

text

Name of the manufacturer.

MeasuredLength

double

Length of ConduitSystem. The ArcFM Length Measured Domain autoupdater uses the MEASUREDLENGTH model name on this field. This field must also be Editable for the autoupdater to work correctly.

Model*

text

Model of the ConduitSystem.

Width*

double

Width of the conduit system.

WorkOrderID

text

Code indicating subtype of ConduitSystem.

IMPORTANT: The following attributes are only valid for the DuctBank subtype (indicated in the table above with *):
  • Height

  • Width

  • Manufacturer

  • Model

  • EncasementType

Configuration field

This single binary large object (BLOB) attribute field of the ConduitSystem feature class stores a COM object containing information describing the layout of the conduit. This includes the value of fields defined in the DuctDefinition object class. Users can create fields in the Duct Definition table such as those listed below. The values of these fields, entered or edited when users place conduits on the map, are stored in the Configuration field. Utility administrators can maintain, query, and edit values in this field.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.