GasPressureSystem

The gas pressure system is a continuous flow system with common Maximum Allowable Operating Pressure (MAOP) and System Operating Pressure (SOP) bound by the Town Border Station, Regulator Station, dead end, or a normally closed valve.

Subtypes: None

Associations: GasSystem, EmergencyIsolationsSystem

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User and designer comments.

GasSystemObjectID

long integer

ObjectID of associated GasSystem.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

MAOPEntered

double

Maximum Allowable Operating Pressure, in any unit of measure.

MAOPStandard

double

Derived field displaying calculated standard Maximum Allowable Operating Pressure.

MAOPUnitOfMeasure

text

MAOP standard unit of measure; examples include psi, iwc, etc.

SOPEntered

double

System Operating Pressure, in any unit of measure.

SOPRange

text

Range of System Operating Pressure.

SOPStandard

double

Derived field displaying calculated standard System Operating Pressure.

SOPUnitOfMeasure

text

Standard unit of measure for System Operating Pressure.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.