EmergencyIsolationSystem

The emergency isolation system is used to isolate a portion of the Gas Pressure System in an emergency. It is bound by a critical, normally closed valve. Any GasPipe can participate in only one Emergency Isolation System at a time.

Subtypes: None

Associations: GasPressureSystem

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.