CPAnode

The anode is connected to the pipe by means of wire and acts as the place of input for the current that is diverted. The anode is “sacrificed” to protect the metal in the pipe from corroding. Anodes are commonly placed at 100- to 1,000- foot intervals along the pipe, depending on the size of the pipe and the weight of the anode.

You may omit specific feature classes from gas traces. To do this, assign the GASNONTRACABLE model name to the CPAnode feature class.

CPAnode acquires properties from the CathodicProtectionDevice abstract class.

Subtypes: None

Associations: CPRectifierCable

Model Names: ANODE, GASNONTRACABLE

Attributes:

Field Name

Field Type

Description

CPRectifierCableObjectID

long integer

ObjectID of associated CPRectifierCable.

CPSectionObjectID

long integer

ObjectID of associated CPSection.

FacilityID

text

Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier.

Material

text

Code indicating material of Anode; domain values include Cast Iron, Galvanic, Magnesium, etc. The MATERIAL model name is assigned to this field for gas tracing.

Quantity

text

Number of Anodes connected to the pipe.

Weight

text

Code indicating weight of Anodes; domain values include 1 pound, 3 pounds, 32 pounds, etc.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.