Sectionalizer Unit

Sectionalizers operate in conjunction with breakers and reclosers to lock out fault current after a predetermined number (usually three) of recloser operations (trips).

Designer uses the DESIGNUNIT model name on this class to designate it as an electric device unit object class. The Designer Work Function Tool uses this model name to identify all electric device unit object classes.

Associations: Sectionalizer

Subtypes: None

Model Names: DESIGNUNIT

Attributes:

Field Name

Field Type

Description

SectionalizerObSjectID

long integer

ObjectID of associated Sectionalizer.

Manufacturer

text

Code indicating manufacturer of SectionalizerUnit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.