Vault

Vaults protect and provide access to underground gas pipes and valves.

Vault inherits attributes from the GasStructure abstract class.

Subtypes: None

Associations: None

Model Names: None

Attributes:

Field Name

Field Type

Description

CoverDiameter

double

Diameter of vault cover (if round) in inches.

CoverLength

double

Length of cover (if nonround) in inches.

CoverWidth

double

Width of cover (if nonround) in inches.

VentingIndicator

text

Code indicating whether vault is vented; domain values include Yes and No.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.