GasStructure

GasStructure is an abstract feature class. GasStructure contains characteristics inherited by Vault and StationStructure that distribute gas to customers.

Subtypes: None

Associations: RegulatorStation, TownBorderStation

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

Contractor

text

Name of contractor.

FacilityID

text

Utility identifier representing a feature’s location in the facility; if the feature is replaced, the new feature has the same identifier.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InServiceDate

data

Date device was set in service.

InstallationDate

date

Date of installation.

LocationDescription

text

Verbal description of location of GasStructure within Facility.

Material

text

Material of GasStructure. Domain values include brick, concrete,steel, etc.

Owner

text

Owner of GasStructure.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

RegulatorStationObjectID

long integer

ObjectID of associated regulator station.

StructureHeight

text

Height of GasStructure.

StructureLength

text

Length of GasStructure.

StructureWidth

text

Width of GasStructure.

TBSObjectID

long integer

ObjectID of town border station.

WorkOrderID

text

Utility-defined identifier of work order.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.