Minerville Autoupdaters

Minerville autoupdaters work only with the Minerville sample data. You may wish to modify these sample AUs for use with your own data. Refer to the ArcFM Solution Developer Help for information about custom autoupdaters.

Component

Description

Used by Classes

Model Names Used

Requirements

Compatibility

Minerville Update Conductor Text

Updates features that have a field with the model name LabelText when constituent conductor unit information changes. This AU subsumes phases with like Conductor Size and Conductor Material. It also places the labels on a single line.

ConductorInfo table

CONDUCTORINFO, CONDUCTORMATERIAL (fmn), CONDUCTORSIZE (fmn)

Enabled when model names are assigned.

Assign To: OnFeatureUpdate

Desktop

Server

Minerville Update Transformer Text

Updates features that have a field with the model name LabelText when constituent transformer unit information changes (looks at two domains: Phase Designation and Transformer Unit kVA).

TransformerUnit table

TRANSFORMERUNIT, LABELTEXT (fmn)

Enabled when model names are assigned.

You can assign this autoupdater only to an On Feature Update event.

Desktop

Server

Minerville Update XFR Rated kVA/Subtype Combo AU

  1. Minerville Update XFR Subtype

  2. ArcFM Update Transformer Bank Rated kVA

Transformer_TransformerUnit relationship class

TRANSFORMER, TRANSFORMERUNIT

Enabled when model names are assigned.

Desktop

Server

Minerville Update XFR Subtype

This relationship AU updates the subtype of the Transformer based on the number of related TransformerUnits.

The Transformer can be of any subtype, such as a single, two, or three phase transformer. When the TransformerUnits (related objects) are added or deleted, this autoupdater modifies the transformer's subtype accordingly.

For example, say there is a transformer with a related object of phase A. If another related object of phase B is later added, this autoupdater updates the subtype from a single phase transformer to a two phase transformer.

Transformer_TransformerUnit

TRANSFORMER, TRANSFORMERUNIT

Enabled when model names are assigned.

Desktop

Server

fmn = Field Model Name

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.