Circuit Source

A circuit (feeder) is the aggregate of the conductors and equipment downstream of a substation breaker or recloser. CircuitSource stores attributes that describe characteristics of the circuit measured or estimated at the breaker or recloser. These attributes include capacity, measured in kilowatts (kW); resistance, measured in ohms; and load, measured in reactive kilovolt-amperes (kVAR).

Associations: BusBar, CircuitBreaker, Recloser

Subtypes: kW, Swing, Voltage Controlled. The use of subtypes is optional. The Subtype attribute can be removed if subtypes aren't used in the model.

Model Names: CIRCUITSOURCE

Attributes:

Field Name

Field Type

Description

BusBarObjectID

long integer

ObjectID of associated BusBar.

ConnectionConfiguration

text

Code indicating configuration of conductors; domain values include Delta, Wye, etc.

DynamicProtectiveDevObjectID

long integer

ObjectID of associated dynamic protective device.

EmergencyCapacitykW

long integer

Emergency rating of CircuitSource, in KW; domain values include 12.

FeederSourceInfo

long integer

Stores information about source of feeder. Feeder Manager requires the FEEDERSOURCEINFO model name on this field. Feeder Manager uses this field to determine whether a feeder has features that participate either loop or multifeed situations.

GroundReactance

double

Reactance of ground seen at the source by the downstream circuit.

GroundResistence

double

Resistance of ground seen at the source by the downstream circuit.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

ID

text

System-generated identifier of feeder initiated at this source. Feeder Manager uses the FEEDERID model name on this field.

MaximumCapacitykW

long integer

Maximum allowable operating capacity of CircuitSource; domain values include 10.

MaxKVAR

long integer

Maximum kVAR load experienced at CircuitSource; domain values include 6.

MaxPositiveSequenceReactance

double

Maximum positive sequence reactance seen at the source by the downstream circuit in ohms.

MaxPositiveSequenceResistance

double

Maximum positive sequence resistance seen at the source by the downstream circuit in ohms.

MaxZeroSequenceReactance

double

Maximum zero sequence reactance seen at the source by the downstream circuit in ohms.

MaxZeroSequenceResistance

double

Maximum zero sequence resistance seen at the source by the downstream circuit in ohms.

MinFaultCurrentOH

long integer

Calculated minimum fault current for overhead conductors.

MinFaultCurrentUG

long integer

Calculated minimum fault current for underground conductors.

MinkVAR

long integer

Minimum kVAR load experienced at CircuitSource; domain values include 500, etc.

MinPositiveSequenceReactance

double

Minimum positive sequence reactance seen at the source by the downstream circuit in ohms.

MinPositiveSequenceResistance

double

Minimum positive sequence resistance seen at the source by the downstream circuit in ohms.

MinZeroSequenceReactance

double

Minimum zero sequence reactance seen at the source by the downstream circuit in ohms.

MinZeroSequenceResistance

double

Minimum zero sequence resistance seen at the source by the downstream circuit in ohms.

Name

text

Utility name of CircuitSource. Feeder Manager uses the FEEDERNAME model name on this field.

NominalVoltage

long integer

Code indicating system voltage for which CircuitSource is rated; domain values include 7.2 kV Grounded Y, 24.9 kV Grounded Y, 2400 Delta, etc.

OperatingVoltage

long integer

Code indicating standard level of voltage at which system is currently operated in kV; domain values include 12.5 kV Grounded Y, 7.2 kV Grounded Y, etc.

SubstationID

text

Substation identifier. Feeder Manager uses the SUBSTATIONID model name on this field to identify the substation that acts as a source.

VoltageAngle

double

Angle at which phase is offset from system standard.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.