PipeExposure

PipeExposure refers to a section of gas pipe that has been exposed.

Subtypes: None

Associations: GasPipe, ExposedPipeInspection

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

CorrosionCode

text

Code indicating degree of corrosion; domain values include None, Light, Moderate, and Heavy.

CorrosionExtent

text

Code indicating extent of corrosion; domain values include General and Localized.

DistributionMainObjectID

long integer

ObjectID of associated Distribution Main.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InspectionDate

date

Date of last inspection.

InstallationDate

date

Date of installation.

LengthExposed

text

Length of pipe that is exposed.

LocationDescription

text

Verbal description of location.

ServiceObjectID

long integer

ObjectID of associated Service.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.