U

UML

Unified Modeling Language. A standard for representing object designs.

Upstream

In tracing, upstream is the direction along the arcs that is against the direction of flow. Direction of flow is determined by a user-defined convention.

User (documents, page templates, stored displays, etc.)

ArcFM allows system and user versions of various layout and map production elements (documents, page templates, stored displays, favorites, etc). Those created by individuals (not administrators) are called User documents, stored displays, etc. They may be created, edited, and utilized only by the individual who created them.

User Role

Defines the capabilities a user is allowed within the process flow. For example, a user with the Approval Officer role, may view sessions and designs with a Pending Approval state and may transition them using the Approve and Reject transitions. Used interchangeably with Role.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.