Regulator

A regulator is a mechanical device used for the controlled reduction of pressure in a gas distribution system.

Subtypes: None

Associations: GasStation, RuralTap

Model Names: None

Attributes:

Field Name

Field Type

Description

Comments

text

User or designer comments.

FlowEquation

text

Equation used for analysis of regulator.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

Manufacturer

text

Code indicating manufacturer of regulator; domain values include American, Fisher, Reliance, etc.

OrificeDiameter

text

Size of orifice.

Owner

text

Owner of associated facility.

PropertyUnitCode

text

Value assigned to assets to track and classify Property Records.

RegulatorStationObjectID

long integer

ObjectID of associated regulator station.

RuralTapObjectID

long integer

ObjectID of associated RuralTap.

SetPressureEntered

double

Pressure at which regulator releases to prevent overpressuring within system.

SetPressureStandard

double

Pressure at which the valve is set to release in system standard units, generally psi.

SetPressureUnitOfMeasure

text

Units in which pressure is measured within system.

SpringRange

text

Indicates the number of units over which the spring on the regulator operates.

TBSObjectID

long integer

ObjectID of associated town border station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.