MeterSetting

MeterSetting represents the geographical location of a meter or bank of meters at service points. Meters measure the volume of gas flow, which is defined by temperature and pressure.

Assign the LOCATABLEOBJECT model name to enable fields for the Object Query Locator tool.

Subtypes: None

Associations: Meter

Model Names: None

Attributes:

Field Name

Field Type

Description

BypassIndicator

text

Code indicating whether meter or meter bank is bypassed; domain values are Yes and No.

Comments

text

User or designer comments.

FacilityID

text

Utility identifier representing a feature's location in the facility; if the feature is replaced, the new feature has the same identifier. Assign the LOCATABLEFIELD model name to enable fields for the Object Query Locator tool. The feature or object class must have the model name LOCATABLEOBJECT assigned.

GasTraceWeight

long integer

Information used for tracing analysis; stored in a bitgate. To support Gas Tracing and Feeder Manager, the model name GASTRACEWEIGHT is required for every feature class belonging to ArcFM gas networks.

Hyperlink

text

Used to store a hyperlink path via standard Esri hyperlinking functionality.

InstallationDate

date

Date of installation.

LocationDescription

text

Verbal description of location of MeterSetting.

LocationID

text

Utility-assigned identifier of the MeterSetting.

Owner

text

Owner of GasDevice.

Premise

text

Foreign key linking to customer information system.

SymbolRotation

double

Angle that dictates how the feature appears on a map.

Subtype

long integer

Code indicating type of GasDevice, examples include Gas Lamp, Relief Valve, and Gas Station.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.