Span Guy

Span guys are installed to span from the top of one structure or pole to the other and offset the strain from the line conductor. Span guys transmit horizontal force to another pole until an anchor guy can be used. SpanGuy is a linear feature and inherits attributes of Guy and Structure abstract classes.

The Structural Analysis tool uses Span Guys while evaluating the amount of guy support necessary for a given support structure.

The SpanGuy class inherits attributes from the Guy and Structure abstract classes. Model names assigned to these classes should be assigned to the SpanGuy class as well.

Subtypes: None

Associations: None

Model Names: SPANGUY

Attributes: None

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.