XML Style Sheets

These style sheets are found in the Bin\Style Sheets folder of the ArcFM Solution installation directory.

Style Sheet

Description

Used by Tools:

ConflictReport.xsl

The ArcFM Mobile Solution uses this report to format the Conflict Report which is displayed when an Enterprise user opens a session or design from the field and it contains conflicts.

Mobile

ConvertCUTypeProgID.xsl

Use this style sheet to convert CU types to ProgIDs.

Designer

ConvertToArcFM9Objects.xsl

Use this style sheet when importing an XML from an earlier release into ArcFM 9.1 or later.

ArcFM Import Tool

CostReport_8_2.xsl

Use this style sheet when exporting the Cost Report in Workflow Manager.

Workflow Manager (Designer only)

DuctQueryReport.xsl

Use this style sheet when exporting the Conduit Manager Conduit Trace Report in ArcMap.

Conduit Tracing

EditHistory.xsl

The Display Edit Log subtask uses this style sheet to display information. It is also applied to the edit log portion of the XML packet.

Process Framework

ExportReport.xsl

Use this style sheet to export database information using the ArcFM Import/Export tool. When you export with this style sheet, save the exported data with an HTML file type and it converts the XML to an HTML report. The HTML report may not be imported back into the geodatabase.

ArcFM XML Import/Export tool

FavoritesReplaceOracle.xsl

Use this style sheet when exporting CUs from an Oracle database and importing into an Access mobile login database (e.g., ArcFMMobileLogin.mdb). This style sheet assumes that ArcFM is the owner of the exported/imported tables. This style sheet strips the unnecessary prefix from the table names before importing them into the field login database for Mobile.

Process Framework Administration Tool Import/Export

Inventory_8_2.xsl

Use this style sheet when exporting the Inventory Report in Workflow Manager.

Workflow Manager (Designer only)

Inventory_9_1_2.xsl

Use this style sheet when exporting the Inventory Report in Workflow Manager. This style sheet consolidates CUs with identical WMS Codes and Work Function values. Linear CUs are given a quantity of 1 and the length if the sum of the individual CUs' lengths.

Workflow Manager (Designer only)

MinerWorkfunction.xsl

Converts domain-driven work functions into string values that are mandated by CIM. This style sheet allows for custom or localized work functions. Resides in Style Sheets\CIM\10.7.

Message Processing

MspAnalysisResultsTemplate.xsl

Internal use only.

Network Adapter

Multispeak_SetUnknownStatusToOpen.xsl

This style sheet converts all instances of "Uknown" to "NO". This is necessary because DMS does not accept unknown switch positions. This style sheet makes the assumption that "Unknown" switch status means "Open".

Network Adapter/DMS

NetAdapter_AddMspScadaPoints.xsl

Reads the ScadaPointID field on switchable devices and adds these points to the XML.

Network Adapter

NetAdapterElecDistToMsp.dtd

This style sheet defines the table names, subtypes, and related tables needed in the Multispeak export for the electric distribution data model.

Network Adapter

NetAdapterElecDistToMsp_Base.xsl

This style sheet contains the generic transformation information used when exporting Network Adapter XML from an electric distribution database and importing it into a MultiSpeak XML.

Network Adapter

NetAdapterElecDistToMsp_DMS.xsl

This style sheet contains the DMS transformation information used when exporting Network Adapter XML from an electric distribution database and importing it into a MultiSpeak XML. This is the top level style sheet and includes the other style sheets and DTDs. The transformation information in this style sheet overrides the information in NetAdapterElecDistToMsp_Base.xsl.

Network Adapter

NetAdapterElecDistToMsp_DMSEquipment.xsl

This style sheet exports the DMS catalogID values where they are populated. It also provides default DMS catalogIDs where needed. The DMS CatalogID field is identified by a field model name.

Network Adapter

NetAdapterElecDistToMspFields.dtd

This style sheet defines the field names of fields that are used in the MultiSpeak export from the electric distribution data model.

Network Adapter

NetAdapterMspDeleteFilter.xsl

Internal use only.

Network Adapter

NetAdapterMspEAExport2.dtd

Defines feature class names, subtype codes, and relationships between unit tables and the circuit source table. This is appended to the NetAdapterMspEAExport.dtd with updates for 9.1 SP1.

Network Adapter

NetAdapterMspEAExport3.dtd

Defines feature class names, subtype codes, and relationships between unit tables and the circuit source table. This is appended to the NetAdapterMspEAExport.dtd with updates for 9.1.2.

Network Adapter

NetAdapterMspEAExport.dtd

Defines feature class names, subtype codes, and relationships between unit tables and the circuit source table.

Network Adapter

NetAdapterMspEAExport.xsl

Use this style sheet to apply to data on export. This style sheet may be customized to change how data is exported. It references NetAdapterMspEAExport_Base.xsl and NetAdapterMspEAExport_Equipment.xsl.

Network Adapter

NetAdapterMspEAExport_Base.xsl

This style sheet was not intended to be customized. It contains the default template used when exporting data. If you wish to modify how data is exported, edit NetAdapterMspEAExport.xsl.

Network Adapter

NetAdapterMspEAExport_Equipment.xsl

This style sheet adds the EquipmentID string to all device and conductor features that don't already have an EquipmentID field.

Network Adapter

NetAdapterMspEAExport_NoConductors.xsl

Sample style sheet for utilities that don't use a ConductorInfo table.

Network Adapter

NetAdapterMspEAExport_NoUnits.xsl

Sample style sheet for utilities that don't use unit tables (e.g., Fuse_Unit, Switch_Unit).

Network Adapter

NetAdapterMspEAExport_VoltageCodes.xsl

This style sheet takes the voltage code domain values from the base style sheet (NetAdapterMspEAExport_Base.xsl) and puts them in a style sheet that may be edited. Voltage code domain values may not be edited in NetAdapterMspEAExport_Base.xsl.

Network Adapter

NetAdapterMspEAExport_VoltageCodes_92sp1.xsl

These Voltage codes were revised for 9.2 SP2 and later. The original values, as they appeared in 9.2. SP1 and earlier, are provided in this XSL for existing implementations. If you wish to use the old values to stay consistent with an existing implementation (on ArcFM 9.2 SP1 or earlier), rename this file to "NetAdapterMspEAExport_VoltageCodes.xsl.

Network Adapter

NetAdapterMspEAExportFields.dtd

Contains all of the field names for all feature classes in the network (except Feeder Manager features).

Network Adapter

NetAdapterMspEAImport.xsl

Internal use only.

Network Adapter

NetAdapterRemoveNANamespace.xsl

Internal use only.

Network Adapter

Prefix_Oracle.xsl

Use this style sheet to export personal (Access) database information into an Oracle SDE geodatabase using the ArcFM Import/Export tool.

ArcFM XML Import/Export tool

Prefix_SQLServer.xsl

Use this style sheet to export personal (Access) database information into a SQLServer SDE geodatabase using the ArcFM Import/Export tool.

ArcFM XML Import/Export tool

pxWorkflow.xsl

Use this style sheet to create an HTML report when exporting using the XML Exporter in the Process Framework Administration Tool.

Process Framework Administration Tool

QAQCReport_8_1_2.xsl

Use this style sheet when exporting an ArcFM QAQC Report in ArcMap. This style sheet can be used to control the encoded scheme used by the QA/QC report. Use the xsl:output encoding element to designate a specific encoding format. For example:

<xsl:stylesheet version="1.0" xmlns:xsl="http://www.w3.org/1999/XSL/Transform">
   <xsl:output encoding="UTF-8"/>

Note that the html meta tag should either match the xsl:output element or be removed entirely. The meta tag is not required, but if it exists it must match the xsl:output encoding element.

ArcFM QA/QC tool

Replace.xsl

Use this style sheet to export SDE database information into a personal (Access) geodatabase using the ArcFM Import/Export tool.

ArcFM XML Import/Export tool

tableAct.htc

Internal use only. Provides JavaScript for some style sheets.

General

WfmDesign_To_CIM10rev7.xsl

Internal use only. Resides in Style Sheets\CIM\10.7.

Message Processing

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.