Delivery Point

Associations: None

Subtypes: None

Model Names: None

Attributes:

Field Name

Field Type

Description

BillingType

text

Type of billing.

DeliveryToOwner

text

Code indicating whether bill is delivered to owner; domain values are Yes or No.

MeterIndicator

text

Code indicating presence of meter; values are Yes or No.

OperatingStatus

text

Code indicating status of DeliveryPoint; domain values include Active and Inactive.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.