Address Search Tab

Use the Address Search tab to jump to a location.

To locate an area by address, follow these steps:

  1. Click the Address Search tab.

  2. If necessary, use the Country drop-down to select your country.

    TIP: A default country can be set in Solution Center > DHFC > Application Settings > General.

  3. Type part (or all) of the address. Then, either press Enter or just wait a moment as the application queries the address automatically.

    TIP: Do you only have a ZIP code or city? That’s fine! The search field accepts any part of the address. The more of the address you have the more accurate the results, but it allows you to jump to a state, a city, a ZIP code, etc. More good news: the field even accepts intersections separated by & or the word “and.”

  4. A list of matching addresses appears. Click the appropriate address.

    • The map moves and centers on your selected address.

    • A location pin is added to the map displaying the address point.

  5. If you are done using the Address Search, click the Clear button to remove the location pin on the map.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.