Arrange a Component

Available for These Components

Notes

Amplifier

Directional Coupler

Power Inserter

Power Supply

Splice

Splitter

Tap

This action is available when two or more components are adjacent to each other.

  1. Right-click the component you would like to re-position, then choose Arrange.

  2. After choosing Arrange, the application waits for you to click the triangle where you would like to position the component.

  3. Click the appropriate triangle, and the application re-positions the component accordingly.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.