View Footprint

Besides Draw Footprint, all the other MDU tools work while viewing the “inside” of an MDU. Thus, clicking View Footprint is the first step toward managing the components inside an MDU. To use this tool:
  1. Click the View Footprint tool. Your cursor changes to include a question mark.
  2. Click the MDU you wish to “open” and view inside.

  3. The application opens the MDU showing you the inside. From there, you can sketch floors, add text, and manage the internal components, stranding, and network.
  4. Click Close to return to the map.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.