Place Strand Tool Hotkeys

While placing stranding, the following hotkeys help with all aspects of stranding.

IMPORTANT: Most computers respect the typical, left-click mouse button when using these hotkeys. However, if you find the application does not let you sketch a structure while pressing one of the hotkeys below, try using right-click to place the structure. This is particularly true on some laptop models.

Action

Key

Align axis horizontally or vertically

A

Cancel

Esc

Disable snapping (when placing two structures close to each other)

Space bar

Lockbox

L

Demarcation point

D

Vertex with underground junction

J

Mid-span pole

M

Set house count on placed component

0 - 9

Snap to MDU border

X

Trench

T

Change to structure type opposite of the default (in other words, if Overhead is the default, Shift changes it to Underground when you click, and vice versa)

Shift

Vertex in underground strand without structure (default is with structure)

Ctrl

IMPORTANT: If you sketch a structure with more than one hotkey pressed, the application does not sketch two structures. Instead, it follows a hierarchy of structure types and places one structure. In the following list, a structure ranked higher “wins” and is placed if more than one structure hotkey is pressed simultaneously:
  1. Lockbox, hotkey L

  2. Demarcation Point, hotkey D

  3. Underground Junction, hotkey J

  4. Pedestal, which could be placed without a hotkey if the Default Structure Type is Underground or placed with hotkey Shift if the Default Structure Type is Overhead

  5. Pole, which could be placed without a hotkey if the Default Structure Type is Overhead or placed with hotkey Shift if the Default Structure Type is Underground

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.