Marquee Select

The Marquee Select  tool allows you to select numerous RF components at once. The Marquee Select does not interact with the stranding network and does not select from the stranding network.

To use the tool:

  1. Click once in the map.

  2. Drag your cursor and notice the application draws a selection box following your cursor.

  3. When the RF components you wish to select are surrounded, click once again. Any RF component that was entirely or partly within the selection box is selected.

.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.