Context Wheel

The right-click Context Wheel provides menu options specific to the component you select. Right-click options are context based. When you right-click a node, for example, you see options that pertain only to nodes. When you right-click a different component, you might see fewer or additional options depending on the component.

The following is an example of the right-click options for various components:

The topics in this section outline right-click options and provide a description of the behaviors available based on the component you right-click.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.