Draw Floors

This tool sketches evenly spaced rectangles. Commonly, it is used to sketch the floors of the MDU, but it can also be used to sketch evenly-spaced units in a horizontal fashion. To use this tool:
  1. First, use the View Footprint tool to see the inside of the MDU.
  2. Once inside the MDU, click the Draw Floors tool. Your cursor changes to a crosshair.
  3. Right-click anywhere inside the MDU to input the number of floors and their orientation, then click OK.

  4. Click once on one of the corners of the building, then move your cursor toward the opposite corner. Notice it displays the floors as you move your cursor.

  5. Click the opposite corner to finish the sketch.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.