Signal One-line Diagram

As you design your network, Designer HFC creates a diagram of the current port leg in the one-line viewport toward the bottom of the HUD.

The one-line diagram displays the current RF leg and all its components. DHFC displays the physical distance between components by labelling the line connecting the icons with the relevant footage. You can click on an icon to have the data for that component display in the left column and to highlight the component's icon on the map.

For a node  component, a plus sign connected to the icon represents the output ports of a node. Clicking a plus sign will target another port of the node. A letter in the lower right of the node icon indicates the port from which that particular leg of the network is connected.

Refer to the Map Symbols topic to understand symbols that display in the one-line diagram.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.