Conflict Resolution

If two different designers simultaneously save changes to the same project file, the file with the most recent timestamp is uploaded.

Typically more than one designer is not designing nor editing the same node.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.