Pads and Equalizers

DHFC selects the optimal pads/equalizers, when appropriate, for your design. If the selected component has internal pads and equalizers, they are listed in this section. If the Swap button is available for a plugin, you can swap it for a different plugin. When you click Swap, a list of all valid plugins available for swapping is displayed. Select a plugin then click OK.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.