Draw Footprint

Drawing the building footprint is the first step toward managing an MDU. To draw the MDU footprint:
  1. Zoom in to the location of the MDU.
  2. Click the Draw Footprint tool.
  3. Click one of the corners of the MDU. The cursor changes to a crosshair.

  4. Move your cursor to the opposite corner of the MDU, then click. The application draws the footprint of the MDU.

    TIP: You cannot change the dimensions of an existing MDU footprint. If you made a mistake while sketching the footprint, click Undo, then sketch again.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.